HTC

Layering Architecture Styles


A traditional way of structuring systems that may also be used to combine architecture styles is layering. In such systems, one set of higher-level functions is implemented using operations provided by a lower-level virtual machine. In architectural terms, this means run-time support for the architecture style used at the higher level is provided at a lower level, where that lower level may use a different architecture style. What often happens in these cases is that the lower level provides run-time support for the interface and coding guidelines of the upper level. The figure below gives an example of this, where a real-time executive layer developed using a concurrent state machine style supports a higher-level real-time process layer. The different events that drive the concurrent state machine correspond to such things as service calls by the real-time process layer, as well as other events such as clock and device interrupts. This approach is used in the implementation of the MetaH language , for example, where all the details of configuring the underlying concurent state machine executive are handled automatically by the tools.

DSSA for GN&C Home Page