HTC

Missile Pitch Axis Example


The problem is to develop control software to help guide a missile towards a designated target. The figure below shows the various missile axes, velocities and forces. Of particular interest here is that the missile can be accelerated in a lateral direction by forcing the missile body to be at an angle with respect to the direction in which the missile is traveling. This is done by controlling the angle of fins located at the aft end of the missile. The resulting aerodynamic force against the side of the missile body causes the missile to accelerate laterally, which is to say causes the missile to turn. The behavior of the missile is modeled using the system of equations shown.

In this simple example we are only going to consider one axis, the pitch axis. We are also going to restrict our attention to that portion of the control software responsible for tracking a desired lateral acceleration.

The figure above shows in solid lines the portion of the overall missile system that will be modeled and developed in this example. A model of the missile is specified and used to simulate the missile dynamics (the response of the physical system to commanded fin deflections). A specification for a control algorithm is developed that commands fin deflections to cause the missile to accelerate along the pitch axis. The missile acceleration tracks a desired acceleration command, which in an actual missile would be provided by a guidance function that will not be discussed here. Software is developed for both a simulation of the missile and for the controller. This software is executed in a real-time hardware-in-the-loop testbed, where the desired acceleration command is injected as a test signal.

The following development steps are performed to produce the various development artifacts. We will present these in a linear order, though in an actual development effort an initial simple specification will be evolved to the final specification based on analysis, simulation and test results.

Specify ControlH Missile Model and Pitch Axis Controller

A ControlH specification of the missile model and an algorithm to control the pitch axis is developed (you can traverse this specification and examine its pieces by selecting objects of interest). Initially the operators in this specification may be simple linear models, where the specification becomes more elaborate as development progresses.

Analyze Control System Behavior

Once an initial ControlH specification is available, a simulation is executed to observe the behavior of the system with various input signals (a simulated response to an acceleration command in this case). Equilibria points of the system or pieces of the system (an equilibria point for the missile model in this example) are determined, linearizations are performed at points of interest, and traditional mathematical analyses such as Bode plots (response of the missile body to fin angle in this case) are obtained from these linear system models.

Generate Source Modules and MetaH Specifications

When the GN&C engineer wishes to start addressing the issues of embedding the control algorithm in an embedded control computer, source code modules together with MetaH specifications that describe those modules are generated. These will appear in the MetaH specification of the overall system.

Generate Test Source Modules and MetaH Specifications

The control algorithm operates on input signals (the acceleration command in this example) to produce output signals (various test signals in this example). In the final system input and output signals are associated with physical I/O hardware such as A/D and D/A converters. For hardware-in-the-loop testing, however, special test code is produced to generate and collect real-time test signals. MetaH specifications that describe this test code are also produced. A tool called the ersatz device generator is used to automatically produce test drivers from a high-level specification of the signals to be injected and collected.

Specify MetaH Integrated System Architecture

The code produced for the missile simulation and pitch axis controller and the test drivers are integrated to form an overall hardware-in-the-loop test system specification. These consist of a MetaH controller macro generated by the ControlH tools, and device processes generated by the ersatz device generator. The MetaH descriptions of these pieces are combined to form a complete MetaH specification of the missile pitch axis simulation and controller system (you can traverse this specification and examine its pieces by selecting objects of interest).

Analyze Computer System Behavior

Once an initial MetaH specification that contains at least estimates of the execution times is available, a schedulability analysis is performed to investigate the real-time properties of the system. We are currently working towards automated reliability analysis for fault-tolerant systems and secure partitioning analysis for dependable systems.

Generate, Download and Execute the System

The MetaH specification of the complete system is used to automatically configure a real-time executive and perform the series of compilations and links needed to produce a load image. Target-specific tools (Adascope for the i80960MC in our example) are used to download the image, execute the system, and retrieve the test results. Data gathered from the execution of the real-time system, such as measurements of the actual process execution times, can be compared against initial estimates and simulation and analysis results to verify correct operation.

DSSA for GN&C Home Page